The General table in the uplink carrier node enables you to turn the uplink carrier on and off, select a saved channel configuration, and view the length of the generated waveform.
The Baseband parameters for the uplink carrier are described in Baseband (Basic LTE FDD Uplink).
Double-click or use the drop-down menu to turn the carrier Off or On.
Select a channel configuration with the desired modulation
type, bandwidth, and number of resource blocks (RB)
from the
drop-down menu.
The setting is not selectable until certain parameters are changed, then is automatically set by the software.
Choice: 1 slot (0.5 ms) | 2 slots (1.0 ms) | … | 18 slots (9.0 ms) | 19 slots (9.5 ms) | 1 frame (10 ms)
Default: 1 frame (10 ms)
Displays the waveform generation length and this parameter is read only. The software sets the Total Sample Points based on the selected Waveform Generation Length and the Oversampling Ratio as below.
Total Sample Points = Base Sampling Rate (MHz) × Oversampling Ratio × 1000 × Waveform Generation Length (ms).
Figure 1 shows the generic frame structure.
Figure 1. Generic radio frame structure
Range: 0 to 19 slots
Default: 0 slot
Sets the waveform generation offset.
When the waveform generation length or offset is set, Waveform Generation Length + Waveform Generation Offset <= 1 frame (10 ms) is automatically satisfied by the software.